Cancel
Showing results for 
Search instead for 
Did you mean: 

Using Alternate Assemblies is not friendly to use

Valued Contributor
Valued Contributor

I am trying to build a complex machine.

which i use alternative position in the assembly .......

Smiley Mad but i am not able to use mirror part ... its really irritating ...i dont want to start the assembly again ...

why dont solid edge have these options ..Smiley Frustrated

MfG -
Viv
11 REPLIES

Re: Using Alternate Assemblies is not friendly to use

Genius
Genius

Hello,

 

Try save assemblie witch severals alternate assembliess (AA) and You will see difference to assieblies witchout AA, this is one of most buged tool in SE.

SE ST9 + TC 10.1.7

Re: Using Alternate Assemblies is not friendly to use

Valued Contributor
Valued Contributor

Yup .. I know that I can do that .... 

but again I get a new assembly name and number .. Smiley Sad

 

 

What I have did is opened a DUMMY assembly  placed the part and made a mirror part in that assembly and saved it ... 

 

and used that Mirror part in my assembly .. 

 

 

verärgert Smiley Frustrated

MfG -
Viv

Re: Using Alternate Assemblies is not friendly to use

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I had to laugh when I saw the title of this post: "Using Alternate Assemblies is not friendly to use..."

The definition of understatement.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Using Alternate Assemblies is not friendly to use

Honored Contributor
Honored Contributor

Mirroring is not nice is cases where you need different details in the mirror, and altertane assemblies is not slick. Combine the two issues.....ouch.

Re: Using Alternate Assemblies is not friendly to use

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bshand You're so right about that!  Maybe we can get @ArtPatrick to fix this stuff.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Using Alternate Assemblies is not friendly to use

Gears Phenom Gears Phenom
Gears Phenom

Yes, you are right. If I remember well, this "new" mirror command was introduced in ST5, but the "old" is in SE yet. This is a little cheat, but a good workaround. You have to customize your UI and place the "old" mirror command.

 

Here is a video about steps:

 

@bshand, sorry for my "magyar" UI! Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Using Alternate Assemblies is not friendly to use

Valued Contributor
Valued Contributor

OFFFFFFFFFFFCOURS !! it works .... thanK you .. that helped me lot ... !  Heart

MfG -
Viv

Re: Using Alternate Assemblies is not friendly to use

Valued Contributor
Valued Contributor

May I have an idea .... For Solid Edge Devlopers or inovaters ....  If there is an option as SAVE as  to SAVE AS MIRROR  in apart tile or a sheetmetal .....

MfG -
Viv

Re: Using Alternate Assemblies is not friendly to use

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Black-Bird wrote:

May I have an idea .... For Solid Edge Devlopers or inovaters ....  If there is an option as SAVE as  to SAVE AS MIRROR  in apart tile or a sheetmetal .....


I think insert part copy along with mirroring in an assembly achieve this, don't they?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200