Cancel
Showing results for 
Search instead for 
Did you mean: 

Using Multiple Coodinate Systems

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I've Been Experimenting Using Multiple Coordinate Systems At Different Elevations. While Using A Line, Curve, Or Whatever Command. Every Time I Try To Aline To The Different Coordinate System... I'm Coming Up With The Same Coordinate Plane.

 

Any Thought. On How To Use Multiple  Plane At Different Elevations

 

Thank you 

GregoryLee

1 REPLY

Re: Using Multiple Coodinate Systems

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Greg,

 

Not sure what your use case is, as to why you need multiple coordinate systems.....but using reference planes is easy.

 

In Synchronous [which is what I think you're using mostly], it's as simple as placing a coincident plane based on one of the base [or existing user defined] planes....then once the steering wheel appears, reloacting [along or about the axis] it as desired.

 

ST8_PAR_Sync_OffsetPlane.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000