Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Using Parts From An Assembly

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Is There A Video Tutorial On Using Parts From An Existing  Assembles.

I Have A Few Parts I Have In One Assembly To Use In Another Assembly

 

Thanks 

Greg

1 REPLY 1

Re: Using Parts From An Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg,

 

Those individual parts in that assembly reside on your computer, in a file directory....so just create your new assembly and add those parts as you want.....it is of no consequense to re-use them elswhere, untill you want to make design changes base on the way the new assembly developes....at which point you then need to use "replace with copy", give it a new name/number and alter accordingly.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000