Cancel
Showing results for 
Search instead for 
Did you mean: 

Using ST7 as default program to open Autocad files with Windows 7

Experimenter
Experimenter

Hi,

 

How can I set the default program to open Autocad files in Windows 7 to be Solid Edge ST7 ?

 

Thank you,

 

 

5 REPLIES

Re: Using ST7 as default program to open Autocad files with Windows 7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

In Windows Explorer, locate an DXF &/or DWG file, right mouse click on it, select Open With, select the Browse button to locate the "EDGE.exe" program executable, found in "Solid Edge > Program" folder, select it, and check the box to the lower left to "Always use the selected program..."

 

Win7_DXFfile_RMC-OpenWith.png

 

Win7_DXFfile_ChooseDefaultApp_SolidEdge.png

 

Win7_DXFfile_ChooseDefaultApp_BrowseToSolidEdge.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Using ST7 as default program to open Autocad files with Windows 7

Phenom
Phenom

Hi,

 

If it doesn't work there is an application that force Solid Edge to point to a specific File Format and it works and it's a FREEWARE!

You have to run the application EXTMAN everytime you need to associate a format file to an application.

http://www.extman.com

It's a german application so you have change the language by clicking on the Icon on the top right after starting it.

For whose intending to donate, the expression Donate isn't translated Man Happy

Donate : Spenden -in German-

 

ExtMan.jpg

 

Yasser

Re: Using ST7 as default program to open Autocad files with Windows 7

Siemens Phenom Siemens Phenom
Siemens Phenom

If you use the right-click -> Open with… solution when opening multiple DXF files from Windows Explorer you will get multiple Solid Edge sessions.

 

The registry settings documented in this post will configure Windows to always open DXF files with Solid Edge *and* force the DXF files to open into a single session of Solid Edge.

 

Edited: Attached the required registry file after the fact for your convenience. Simply download the attached file, double-click to install it, and Solid Edge will always open DXF files into a single session of Solid Edge.

Re: Using ST7 as default program to open Autocad files with Windows 7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@uk_dave wrote:

If you use the right-click -> Open with… solution when opening multiple DXF files from Windows Explorer you will get multiple Solid Edge sessions.

 

The registry settings documented in this post will configure Windows to always open DXF files with Solid Edge *and* force the DXF files to open into a single session of Solid Edge.

 

Edited: Attached the required registry file after the fact for your convenience. Simply download the attached file, double-click to install it, and Solid Edge will always open DXF files into a single session of Solid Edge.


 

Hi Dave,

 

Don't recall which post it was, but, did you notice the request for the ability to be able to reverse this registry action?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Using ST7 as default program to open Autocad files with Windows 7

Siemens Phenom Siemens Phenom
Siemens Phenom
Sean, thanks for the heads up. Been busy of late verifying ST8 PRs and haven't been staying up to date on the forum posts. Anyway, found the post you mentioned and have responded. Cheers!