Cancel
Showing results for 
Search instead for 
Did you mean: 

Using property text to create a driven feature

Phenom
Phenom

I have a bunch of 3D printed parts that have their revision letter embossed on a surface. Is there any way I could have the revision property text drive the sketch and feature? I realize it'll have to be in ordered.

 

Harri "synchronous"

3 REPLIES 3

Re: Using property text to create a driven feature

Gears Phenom Gears Phenom
Gears Phenom

We can use property text as PMI but I do not believe you can use it as a feature.

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Using property text to create a driven feature

Phenom
Phenom

@Johnson_BigMatt , this is what I think too, but hoping someone has written a macro or something. There appears to be an ER #1886111 requesting this functionality..

Re: Using property text to create a driven feature

Gears Phenom Gears Phenom
Gears Phenom

This is an old ER! Smiley Sad

 

BR,

Imics
http://solidedgest.wordpress.com/