Cancel
Showing results for 
Search instead for 
Did you mean: 

Using the drafting environment to populate an inspection table

Experimenter
Experimenter

Maybe this has already been answered somewhere but my project is as follows:

 

I have already made a 3D part in metric

I have already used the ansi draft environment to dimension in american units.

Now, I'd like to make an ordered list that uses points on the part as a guide for quality control.

Then I'd like to create a table from that list so that the inspector can sign off that the feature is within the acceptable tolerance.

It'd also be nice if I could reference a tool number easily but that isn't a priority.

 

I played with the different buttons trying to figure it out on my own but I just simply don't know the program well enough to get it to do what I'd like it it.

Any help?

Thanks!

1 REPLY

Re: Using the drafting environment to populate an inspection table

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Something like this?

SE Inspector

 

BR,

Imics
http://solidedgest.wordpress.com/