Cancel
Showing results for 
Search instead for 
Did you mean: 

Using the sheet metal functionality in the part?

Valued Contributor
Valued Contributor

I want to use the etching sheet metal features in the Part environment.
But it can only be used on the metal plate.

I am using the Edge ST9 version.

 

See the picture below

This feature does not seem Etch....

Etch Waht.png
Is

 

there any way in the Part environment?
please improvement.

 

4 REPLIES 4

Re: Using the sheet metal functionality in the part?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Hclee,

 

How will you be using this?.....ie; are you actually getting it laser etched??.....is it a PAR model, of a Sheet Metal item??? [in which case, use the "Switch To - Sheet Metal" command]

 

The etch command in Sheet Metal, is extracted from a planar sketch designed to survive flat patterning out, for use by CNC etching capable machinery......I would think, if it was an equivelant in the part environment you required, then it would be just as it was before etch came along....by placing/projecting a sketch onto the model.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Using the sheet metal functionality in the part?

Valued Contributor
Valued Contributor

I do not want to switch to the sheet metal.
Etch just want to use only the features in the part.

Highlighted

Re: Using the sheet metal functionality in the part?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

If you don't want to switch to SM environment, then I suggest using derived curve...

 

Here is a short video:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Using the sheet metal functionality in the part?

Valued Contributor
Valued Contributor

Good!!

I think you know a lot of features

Thank you for answers.