Cancel
Showing results for 
Search instead for 
Did you mean: 

VBA For File Properties

Experimenter
Experimenter

Hello VBA Experts,

 

I have one excel file with some properties. I need a VBA code to update the active Solid Edge file properties. And it should take all the values from the excel sheet.

 

If I run the VBA code from excel, then only the "ACTIVE SOLID EDGE FILE PROPERTIES" Should Update.

 

BTW I am using SOLID EDGE ST7. Attached file is for your referecne.

 

Thanks in Advance,

 

Regards,

RAY

Regards,
RAY
1 REPLY

Re: VBA For File Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This would be better posted to the Solid Edge Developer Forum since it is referring to programming with the Solid Edge API.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com