Cancel
Showing results for 
Search instead for 
Did you mean: 

VErtical and horizontal curve

Genius
Genius

Hi,

We need to draw a line in a sketch that bends virtically and horizontally at the same time. We were able to do this using a bent surface, a sketch and wrap sketch. But there's a part of the sketch that is left out and doesn't wrap. Here is the .par of it.

Can anyone help fixing this or is there an other way of going about it?

Thanks

ST9
Conveyor and industrial equipment designer.
Giving SE a chance.
14 REPLIES 14

Re: VErtical and horizontal curve

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm no expert with surfaces by any means but if you remove the arc from the sketch and replace it with a line the full wrap appears.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: VErtical and horizontal curve

Genius
Genius

Yep, but we need the radius, that is the problem.

ST9
Conveyor and industrial equipment designer.
Giving SE a chance.

Re: VErtical and horizontal curve

Genius
Genius

Plus, I don't think the problem is in the surface. The same thing happens when you wrap the sketch on a protusion feature.

ST9
Conveyor and industrial equipment designer.
Giving SE a chance.
Highlighted

Re: VErtical and horizontal curve

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yeah, I see. I didn't think it through.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: VErtical and horizontal curve

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Easy on the kudos, man. I didn't really deserve any. Smiley Happy

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: VErtical and horizontal curve

Genius
Genius
Haha!
ST9
Conveyor and industrial equipment designer.
Giving SE a chance.

Re: VErtical and horizontal curve

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Pedneault75,

 

Could this be purely because of the size of the model? ....remembering there is a Parasolid 1Km cubic entity limitation, about the origin, which your part exceeds. Can you break it down at all?

 

Also, I ran the geometry inspector, and it returned the following errors.....[not sure if they are relevant, or related to the size limit]

 

Capture.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: VErtical and horizontal curve

Phenom
Phenom

I can't open your file(ST8?) so can't comment on the curve sizes or error.

However, I can suggest using a Cross Curve as an alternative method.

Just create the 2 curves as sketches then select Cross on the Surfacing > Curves group.

No need to create surfaces or wrap sketches etc, it just creates the inferred intersection of 2 extruded surfaces.

 

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: VErtical and horizontal curve

Gears Phenom Gears Phenom
Gears Phenom

Just for a test i did downsized the model (all the dimensions divided by 1000) and the curve appear correctly now.

 

curve.png