Cancel
Showing results for 
Search instead for 
Did you mean: 

Variable Colors

N/A

Is there a way of adding colors to an individual piece of a part as well as adding variable colors instead of the same plain Jane colors.

Thanks

2 REPLIES

Re: Variable Colors

N/A
the command you are looking for is "part painter". You can paint faces, feature, body...

Regarding a "variable color" my best attemp would be to create an image of your desired variable color as a patch and apply it as a texture.???

HTH

Re: Variable Colors

N/A
Yes, and yes.
Part Painter will allow you to paint a body, feature, or surface. The
colors that you can choose from are defined in the Style settings.
You can create custom 'colors' in the Style, Face Styles settings.
HTH,
Jason
Jason Inglis
The Charles Machine Works, Inc.
Ditch Witch
Perry, Oklahoma
On 1/17/2013 3:32 AM, Crouse@Concept-Dwgs.com wrote:
>
> Is there a way of adding colors to an individual piece of a part as well
> as adding variable colors instead of the same plain Jane colors.
>
> Thanks
>
>