Variable units

Honored Contributor
Honored Contributor

How do I assign units to a variable?

Say I create a variable X

I set it = 1

It thinks it's 1 degree instead of 1 inch. 

How do I controll that?

1 REPLY

Re: Variable units

Esteemed Contributor
Esteemed Contributor

When you create it, the combobox in the upper left corner of Variable Table sets the units.  After it is already created, select the line for the variable by clicking in the Type column and then change the combobox in the corner to the correct type (distance is default).


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3