Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Variables with if/then rules

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RBliss  Yes, ST9 added IF() as well as the inverse trig functions ASIN(), ACOS() and functions to convert between Radians() and Degrees().  Also new is a Variable Rule Editor for Limits and Discreet Lists rules.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Variables with if/then rules

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It would be even easier if the first comma was actually "then" and the second one "else". But that's just a quibble.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Variables with if/then rules

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I'd like to share a 15 minutes video that shows the various posible ways in which the IF function can be used in the Solid Edge variable table:

http://www.surfandcode.in/2016/10/solid-edge-video-quick-tip-059_12.html

 

IFWays.png