Cancel
Showing results for 
Search instead for 
Did you mean: 

Very slow performance ST9 MP6

Legend
Legend

Hi,

 

This afternoon I was working on a assy with 37000+ parts and the performance was "down", I produced a simpel drawing (topview) and the size was 30mb saving to the server took 4-5 minutes... also saving the assy took more than 5 minutes..

 

Than I saved the same drawing to my local SSD drive.. no difference..  also 4-5 minutes...  that was strange...

 

Than I copied this file from local SSD to the server  (30mb) this was done in 1-2 second... so the connection to the server seems to be oke..

 

I run the latest i7 with Windows 10, 32 GB memory, samsung pro 960 SSD and an M4000 quadro card..   ST9/MP6 and ST10 build .78 in dual install mode.

 

Checked the same assy on another workstation Win7 with 96GB memory and saving took also ages..  ST9/MP3

 

Got my modifications done.. but it took more time than expexted due to these delays...

 

Anyone out there with an idea what could be wrong ?

 

Thanks in advance for your help,

 

 

Jan Bos

Emmen, The Netherlands

User since V3.5 beta testing ST10

 

 

 

 

 

 

 

 

1 REPLY

Re: Very slow performance ST9 MP6

Legend
Legend

Just to let you know that I have solved my problem...

 

I have removed ST9 and ST10... removed them from registry... reboot and reinstalled ST9.

 

Clean install   load 8 sec.  save 8 sec.

ST9 MP6  load 8 sec.  save 8 sec.

Dual install ST10 build .78  load 8 sec.  save 8 sec.

 

Somehow I have corrupted my installation.. re-installing solved it..

 

Reg.

 

Jan