Cancel
Showing results for 
Search instead for 
Did you mean: 

View Position

Genius
Genius

Hi.

 

When placing a view on draft, is it possible to fix its position?

 

I am asking because I am driving the model from excel and also driving the scale on the draft.

I want to minimize editing.

3 REPLIES

Re: View Position

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can open the View's properties and check the option "Lock drawing view position".  It is located towards the bottom of the General tab.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: View Position

Genius
Genius

Hi Ken.

 

Thanks for this information.

 

The problem with using this positional lock is that it locks the center of the part, so If I want to produce a parallel key and change its length it will expand in both directions.  I wan to be able to fix one end so that the length will only move one way.

 

I hope you understand what I am asking.

Highlighted

Re: View Position

Genius
Genius

Is this possible?