Cancel
Showing results for 
Search instead for 
Did you mean: 

View Position

Valued Contributor
Valued Contributor

Hi.

 

When placing a view on draft, is it possible to fix its position?

 

I am asking because I am driving the model from excel and also driving the scale on the draft.

I want to minimize editing.

3 REPLIES

Re: View Position

Esteemed Contributor
Esteemed Contributor

You can open the View's properties and check the option "Lock drawing view position".  It is located towards the bottom of the General tab.



Ken

Production: ST10 MP5
Testing: SE 2019

Re: View Position

Valued Contributor
Valued Contributor

Hi Ken.

 

Thanks for this information.

 

The problem with using this positional lock is that it locks the center of the part, so If I want to produce a parallel key and change its length it will expand in both directions.  I wan to be able to fix one end so that the length will only move one way.

 

I hope you understand what I am asking.

Re: View Position

Valued Contributor
Valued Contributor

Is this possible?