Cancel
Showing results for 
Search instead for 
Did you mean: 

View Styles

N/A

Hallo,
I cannot exchange a status of the solid body by cliking on icons in view styles label.
Additionally, when I make a sketch and extrude it there is no visible body at all.

Is that related to hardware of my computer or installation problem?
I have RAM Memory 1GB, Processor 1,66GHz, 512KB Cache!

Regards

Davor

2 REPLIES

Re: View Styles

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Davor,
Not sure what graphics performance your machine has ....but it does sound as though it could be the issue.
You might try, while in an open model file, looking at File>Solid Edge Options>View....on that dialogue, at the top left,..."Application Display", un-check the Automatic selection....and choose "Backing Store" , and see if one of these lets you continue.
If it does work in B-Store, then you may also see lesser performance in this mode.
Hope this helps.....
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: View Styles

N/A
Thank you .

I have it.

I`ll get drink from me.

Best regards

Davor from Zagreb, Croatia