Cancel
Showing results for 
Search instead for 
Did you mean: 

View configuarions in Solid Edge viewer

Builder
Builder

I cannot fing the view configurations option in solid edge viewer, please can someone tell me where this is, very frustrating

3 REPLIES

Re: View configuarions in Solid Edge viewer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Help says you can right-click on the assembly and pick display, etc. but I don't see it.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: View configuarions in Solid Edge viewer

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,
since ST5 this function is no more in SE Viewer or in View&Markup.
Only way I found to "replace" this function is PMI views.

 

Look here for details: Link

 

Ota

Highlighted

Re: View configuarions in Solid Edge viewer

Builder
Builder

I had also seen this in the help information but it was not there Smiley Frustrated