Cancel
Showing results for 
Search instead for 
Did you mean: 

Wacom graphics tablet - use of

Experimenter
Experimenter

Does anyone use a Wacom graphics tablet?

 

I use it instead of a mouse for everything apart from one thing.

 

Quick pick

 

The trouble is a can't keep my hand (the pen) perfectly still, long enough.

 

Does anyone have a solution?

 

3 REPLIES 3

Re: Wacom graphics tablet - use of

Phenom
Phenom

I feel your pain. 

 

I have the timeout on the minimum and have a mouse on my left hand. Just for quickpick.

Next to this I changed the "shift" button of my SpacePilot Pro to "left mouse button".

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
Highlighted

Re: Wacom graphics tablet - use of

Experimenter
Experimenter

thanks Joris

 

Adjusting timeout is good.

 

I've just remembered the tablet is finger touch sensitive too so I can hold the pen and touch with two spare fingers to call up the Quick Pick then continue with the pen

 

pinching and spreading with my fingers zooms too

Re: Wacom graphics tablet - use of

Phenom
Phenom

It would be an interesting test to see if you could setup an inexpensive tablet like the Surface (not Pro) as an "original" tablet- like in the days of early 90's. Here you could have icons on the screen instead of the laminated paper template.