Cancel
Showing results for 
Search instead for 
Did you mean: 

Want to start with ST8, why should or not install it

Dear SE believers Smiley Wink

 

I have been offline for a while due heavy projects, so sorry for that and the questions below. However I don't want to spend hours reading if we should already install ST8.

 

Normally we install with every new release SE, until now we had many start-up problems (first real version was ST7 that worked perfect from the start).

 

Are there problems that will slow down our work process or does it work good (with some minor problems)?

Are there minor problems? And if yes, what are the minor problems?

Are there positive new features that work really good?

 

I really want to know this, so if you could reply it would be really appreciated Smiley Very Happy

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10
19 REPLIES

Re: Want to start with ST8, why should or not install it

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Daniel,

 

ST8 has been performing solidly for us since the release, even with my later leap into Windows 10, it continued to function as expected.....also, MP1 has been released, and it has fixed a few anomolies that I hadn't even encountered.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Want to start with ST8, why should or not install it

Hi Sean, thank you for the reply.
So until now no problems like strange crashes?
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Want to start with ST8, why should or not install it

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Daniel,

 

Nothing that I can attribute to Solid Edge alone, more my own doing, so no, nothing.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Want to start with ST8, why should or not install it

That is also something Smiley Wink
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Want to start with ST8, why should or not install it

Legend
Legend

Hi Daniel,

 

We are using it from day one that it came available through the download (07-06-15), and I have done the remote beta for ST*, we had no problems at all.

 

Kind regards,

 

Jan Bos

Geha

The Netherlands.

 

 

 

 

 

 

Re: Want to start with ST8, why should or not install it

Genius
Genius
Hello, I wanted to join the question. How ST8 cooperation with Teamcenter, if there are any problems that were not in ST7, whether on the contrary it is much better ?
SE ST9 + TC 10.1.7

Re: Want to start with ST8, why should or not install it

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

W10 is not yet supported by Siemens, so the advice for now is to use W7 or W8.

Re: Want to start with ST8, why should or not install it

Gears Phenom Gears Phenom
Gears Phenom

I installed ST8 the moment it was available.

It works solid, but gives some time-out in assembly after selecting a part. This is new for me since ST8.

I havan't found any real improvements (yet?).

...........................................................................................................
Solid Edge ST10 & AutoCAD 2019 user

Re: Want to start with ST8, why should or not install it

Dank je @Joris. Als jij er al tevreden over bent moet het wel de moeite waard zijn

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10