Cancel
Showing results for 
Search instead for 
Did you mean: 

Weird cutting plane (draft) problem

Valued Contributor
Valued Contributor

Hi,

 

I need to place a cutting edge (for a section view), 25 mm. from the end of my part, but Solid Edge change the dimensions to 50% of the correct value.

 

See video:

 

I can probably just type "12,5" in the example video above, but that just feels wrong - to type a false value.

5 REPLIES 5

Re: Weird cutting plane (draft) problem

Phenom
Phenom

It seems, that the cutting plane calculates its position in function of your actual scale 1:2

 

Yasser

Re: Weird cutting plane (draft) problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What's the scale of the view? With sections Edge uses the sheet dimension, not model dimensions in these cases. So it multiplies the dimension by view scale. You can easily see this by changing the view scale then editing the section line. The dimension you place and gets recalculated is the correct dimension in terms of the model at its scale.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200
Highlighted

Re: Weird cutting plane (draft) problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

If you need an exacting location for section lines, I normally just use relationships when drawing the cutting plane profile, but have also used sketch geometry placed within "Draw In View", then locating the cutting plane profile to match that sketch, with relationships as needed.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Weird cutting plane (draft) problem

Valued Contributor
Valued Contributor

The relationship idea was great, worked perfectly Smiley Happy

Re: Weird cutting plane (draft) problem

Valued Contributor
Valued Contributor
It can also help to show hidden lines on the view FIRST before trying to place (and relate to geometry) a cutting plane line.
sryp

ST7 Classic MP0 | Win7