Cancel
Showing results for 
Search instead for 
Did you mean: 

Weld Callouts

When I create a weldment and apply welds in the 3D model, is there a way to pull that into the drawing without having to manually add a new weld callout at the drawing level?  Similar to feature callout for holes.

 

Capture.PNG

Capture1.PNG

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments
3 REPLIES 3

Re: Weld Callouts

Gears Phenom Gears Phenom
Gears Phenom

Far RH option on the Weld Callout Command bar!

5-11-2017 9-44-37 AM.png


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Betreff: Weld Callouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @scott_lester

 

 

 

You can do this with activating the "Weld Symbol - Tie to Geometry" button

 

20170511_1549.PNG

regards
Wolfgang

Re: Weld Callouts

I knew it was something simple.  I dont do many welding drawings and just picked up a client that does all only welding, so I have a little bit of a learning curve Smiley Wink

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments