Cancel
Showing results for 
Search instead for 
Did you mean: 

Weld symbols question

Phenom
Phenom

Hi,

This isn't really so much a software question, though I suppose it can be.

So we have this customer, and though their drawings generally look good visually, theres always a bunch of mistakes we have to find and figure out, no biggie. So but we've kind of determined that the owner of this customer is getting frustrated with us constantly calling or emailing with questions, related to their mistakes, most likely because he drew these and takes it personally.

 

So that's why I can't ask the customer this.

 

Does anybody know what the '0' and the '1' represent in the tail of this symbol?

EDGE QUESTION WELD SYMBOLS.JPG

and to make this software related, anybody know how to get edge to show these digits in the symbol?

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
8 REPLIES

Re: Weld symbols question

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

it is easy. Open properties of weld symbol in draft (or in asm for Weld symbol).

Type desired information into right box next to image of weld symbol (see the pics.)

 

Unfortunately I do not know what informations represents.

 

Ota

Re: Weld symbols question

Legend
Legend
12 years of doing fab design, never seen anything like that.

Re: Weld symbols question

Siemens Phenom Siemens Phenom
Siemens Phenom

What you could do is ask the customer what dimensions and welding symbol standards they are drafting to and to provide a copy of those standards to clarify.  That or when you know what standard they state they are following go purchase your own copy.  Either way, if the schema used doesn't match the standard they claim to be following...

Re: Weld symbols question

Phenom
Phenom

I have never seen a symbol with the 0 & 1 like that before.

 

I would also point out that the size of the fillet is not defined. Perhaps the intent is to place as a large of a fillet as the joint will allow, but I don't like to leave a weld open to interpretation like that. 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Weld symbols question

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I would also put the question up on EngineeringTips.com in the welding thread or drafting thread.  I've never seen these in a welding symbol either.  Here's the link:

 

http://www.eng-tips.com/index.cfm

 

Kyle 

Kyle Joiner
IPA LLC
ST10 MP1

Re: Weld symbols question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have no idea what that might mean. I've never seen the tail used that way. It's possibly an internal standard of their own.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Weld symbols question

Honored Contributor
Honored Contributor

This is a guess, but from the picture, the weld needs to be all around the tube and a seal weld. I would assume 1= all of the connection 0 = nothing. So the other guess of the largest fillet I believe is right and I would add that 1 is the equivalent of 12-12 or 12" of weld every 12 inches. It's very common to see say 1-6 or 1" of weld every 6". They may do this with a 0-1 value or a normalized percent of the contact to be welded.

 

For a reel answer, you have no choice but to ask the company.

Re: Weld symbols question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

My understand is that the Tail can contain anything.  It is suplemental to the symbol to be useed for additioanl instructions or refrence to other documentation.  It may be used to specify what filler rod to use or an internal specification document or other information.  That being said, you will definetely need to have the company that defined the symbol define the annotation used.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com