Highlighted

Well, this is funny. Include is doing ummmm can't explain

Phenom
Phenom

Thank Heavens we have the ability to record short videos, otherwise I would have a hard time explaining this. Using include in a flat pattern. Selecting the element include happens on the side opposite of where I'm selecting. Watch vid.

(view in My Videos)

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
7 REPLIES

Re: Well, this is funny. Include is doing ummmm can't explain

KennyG 2nd Gear
2nd Gear

That's interesting... Looks like an IR.



Ken

Production: ST10 MP3
Testing: SE 2019

Re: Well, this is funny. Include is doing ummmm can't explain

SeanCresswell 2nd Gear
2nd Gear

@nominus38,

 

Oh boy, that really is messed up!........definitely time for GTAC.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Well, this is funny. Include is doing ummmm can't explain

Tushar 2nd Gear
2nd Gear

Hi @nominus38

 

Is it possible to share that file ?

 

Thanks.

 

Tushar

Re: Well, this is funny. Include is doing ummmm can't explain

Phenom
Phenom
I do experience such things in different situations.
The common thing is "edit in place", part where previously edited not in place.

It seem that assembly doesn't get edited geometry in some circumstances.

I get used to close and reopen the assembly when this occour, I would be happy for sure if it gets fixed

Re: Well, this is funny. Include is doing ummmm can't explain

Honored Contributor
Honored Contributor

Par for the course.

 

Sketches still flip. SE crashes frequently, and  Models fall apart all the time for me.

 

I wish I had the time to file more IR's.

Re: Well, this is funny. Include is doing ummmm can't explain

Genius
Genius
I've used a lot of different software, for numerous manufacturing purposes. There is NEVER one software that does everything you want it to do, or doesn't have some quirks. Once you get some years under your belt, you learn to determine what your needs are, work with the software that best meets your needs, and accept how to work around the quirks.

Re: Well, this is funny. Include is doing ummmm can't explain

Phenom
Phenom

Sorry that I haven't responded to this earlier but I've been busy. Not sure if I can upload this one for a number of reasons, but one being the amount of interpart links going on here, and also the whole confidentiality thing. When I get time I'll see if I can strip this thing of it's links and remove customer info. No promises.

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"