Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: The zero thickness error means that whatever geometry you...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

 and if a Synch part you can edit anything as if the part is opened or in edit mode

@KennyG, Could you please explain how?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: The zero thickness error means that whatever geometry you...

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

This can even show up in Drafting.

If you create a section view and accidentally make your cutting line tangent to a hole.

Seems funny but I think it employs Parasolid to do this.

NonMan.PNG

LMGi
www.TLMGi.com

Re: The zero thickness error means that whatever geometry you...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make sure Select in Assy is set to "Face Priority" and select the faces... Edit away!  Best thing about it is that you can select multiple faces across multiple synch parts and edit them all at the same time.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: The zero thickness error means that whatever geometry you...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@KennyG, Thanks. Missed that in my continuing sync education.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: The zero thickness error means that whatever geometry you...

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

My understanding is that Parasolid can quite easily model non-manifold geometry but that it was an executive decision by the developers to not allow non-manifold geometry in Solid Edge because it is non-manufacturable.

Re: The zero thickness error means that whatever geometry you...

Phenom
Phenom

Here is an example of thickness error ...

The lower line of the new sketch is coincidence with the upper one of the 3D model.

 

Yasser

 

zero_thickness_error.jpg

Re: The zero thickness error means that whatever geometry you...

Creator
Creator
Agree completely - I am currently using ST9, I have this error now and there is the potential of a hundred or more... obviously it is most likely 1 spot, but trying to find that one spot is like a needle in a haystack.
There needs to be added functionality - perhaps a special tool in Inspect, in the Evaluate section - or adding an evaluate section into the Sketch tools that includes this functionality.
Something needs to be done.

Re: The zero thickness error means that whatever geometry you...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can have zero thickness or non-manifold features if they are in separate bodies in a multi-body part.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200
Highlighted

Re: The zero thickness error means that whatever geometry you...

Creator
Creator

That was the work around that I just used to be able to move on, creating a New Body.  I'm just happy that this isn't a part that I am having to design for us to make.  It is an injection moulded plastic part - having never worked with injection moulding before, I don't know if a multi-body part would work for that.
Still though, I would have spent FAR less time on this if there was something as simple as the line that was the problem being changed colors for easy location.  Minutes instead of hours.

Re: The zero thickness error means that whatever geometry you...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have no issue with wanting more hints from the software. Surely it must know where the problems lie. Or maybe not IDK.

If you attempt to union the bodies it will show you the problem area. This is a little late though.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200