Cancel
Showing results for 
Search instead for 
Did you mean: 

What happened to lofted surface?

Gears Phenom Gears Phenom
Gears Phenom

When did lofted surface disappear. I even for a minute thought I was crazy and that maybe it never was there, but I have a part open right here that has a lofted surface in it, and I can't figure out how to create a new one of these.

surface loft.JPG

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
4 REPLIES 4

Re: What happened to lofted surface?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hmmmmm.... Not sure of the details but my guess is that maybe Lofted Surface command is obsolete seeing that Blue Surf can do everything a Lofted Surface can do plus more.... unless I'm missing something...

 

 

Kevin Grayson
Solid Edge Technical Consultant
kevin.grayson@siemens.com

Betreff: What happened to lofted surface?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @nominus38

 

 

 

"Lofted Surface" still is there.

 Maybe it was taken from the standard Surface Tab but You can add it via customization of the tabs, using "All Features" and scrolling to "Loft Surface"

 

I have it here in my surface tab, but cann't say wether or not I put it on or it was there by default.

 

 

regards
Wolfgang
Highlighted

Betreff: What happened to lofted surface?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

...

 

 

PS.:

for certain situations "Lofted Surface" does a better job than "Blue Surf"

This is the reason why I have it on my tabs always!

 

 

regards
Wolfgang

Betreff: What happened to lofted surface?

Siemens Phenom Siemens Phenom
Siemens Phenom

It is no longer there by default -- it is a "hidden" command that you must add back in through the theme customization.