What is Axis Lock Direction for Solid Sweep Feature in ST9

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi Edgers,

 

I can't understand what is axis lock direction when using Solid Sweep in ST9. Seems like confusing how to use this feature. First 3 step is okay, but it come to axis lock it always failed.

 

Refer image i snapshot.

 

Anyone can help me. Thanks a lots.

1 REPLY

Re: What is Axis Lock Direction for Solid Sweep Feature in ST9

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:xid1168670

 

Setting the Axis Lock Direction

If the tool is perpendicular to a 2D path, the Axis Lock Direction is set by default. For 3D paths and 2D paths where the tool axis is not perpendicular to the path, the Axis Lock Direction needs to be defined. Axis Lock Direction can be defined by the direction of edges, feature axes, coordinate system axes, or planes.

 

HTH

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6