Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

What is going on with Standard Parts in ST7

Master
Master

In the beginning we worked with Standard Parts V10.0.

With the new installation of ST7 and the standard parts administrator. For some reason I needed to import all the part again in the SQL server (or what ever it's name is). Eureka, it worked.

 

Now with ST7 and MP1 and MP2, all the selected standard parts are regenerated in V12.0. That's strange right?

But also, no thread is shown on the bolts and nuts.

 

Now I really want to know what is going on

2 REPLIES 2

Re: What is going on with Standard Parts in ST7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

yes, I astonished see that the thread really is away.

 

Going into the part itself shows, that the thread feature seems to be corrupted.

I suppose this has to do with the new hole tables.

 

Defining the thread manually will bring it back immediately.

 

Must be solved quickly

Does anybody know wether there is an PR or not

 

 

regards

Wolfgang

 

 

regards
Wolfgang

Re: What is going on with Standard Parts in ST7

Master
Master
I have made a request for a PR by my reseller.
Hope I get some feedback.