Cancel
Showing results for 
Search instead for 
Did you mean: 

What is included in solid edge classic

Experimenter
Experimenter

So i am installing SE on a new computer, and it seem like the discs I have contain all the add-ons applications that Siemens offers. I have a node lock version of SE classic and i am wondering what applications i should install? 

 

so like on the 1st disc(windows 64-Bit) there is this option window in place

Select the SE products you would like to install 

 

Solid edge (done that and have the licensing key finished too)

 

Electrode design

Mold tooling 

Standard parts administration

Data migration 

 

SE SP Client

SE Teamceter Client

SE Insight Client 

 

license manager

dongle driver 

 

what of those do i need to install on my computer with a node lock classic versions of solid edge ST8

 

on the 2nd disc(data management) there is this option window in place

 

Solid Edge Product Installation

 

 

Solid Edge Data Management Applications

 

Select the Solid Edge product you would like to install:


 32-bit applications
» Insight Connect
» Solid Edge Viewer
» Solid Edge Teamcenter Administrator 

 

64-bit applications
» Solid Edge SP Client Standalone
» Solid Edge SP Server 2010
» Solid Edge SP Server 2013
» Teamcenter Structure Editor
» Insight Server 2010
» Insight Server 2013

 

on the 3rd disc(standard parts libraries) there is this option window in place

 

Solid Edge Standard Parts Libraries

 

Select the Solid Edge product you would like to install:

Solid Edge Install Logo

» Machinery Library
» Piping Library

8 REPLIES

Betreff: What is included in solid edge classic

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


the ionly extras You can run with Classic will be the standard parts with Machinery Lib and insight Client, as well as the engineering reference

 

Mold and Electrode are extra modules

 

License manager and dongle driver are not necessary for node locked license since node locked will use the SEID the Solid Edge Identification hardwre number

 

regards

Wolfgang

 

regards
Wolfgang

Betreff: What is included in solid edge classic

Experimenter
Experimenter

thank you 

Re: What is included in solid edge classic

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Here is a matrix of the differences....

 

SE-Features-Chart.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: What is included in solid edge classic

Builder
Builder

Does anybody know what the approximate price is in the U.S. to add the piping library to a premium license?

 

Re: What is included in solid edge classic

Valued Contributor
Valued Contributor

I think xpress route should be included as standard Smiley Wink 3D sketch is nearly there...

Re: What is included in solid edge classic

Builder
Builder

Yes, Xpress route is, but I was told that the piping library was a seperate item.

 

Re: What is included in solid edge classic

Community Manager Community Manager
Community Manager

Your sales partner should be able to provide you local pricing. Do you know who that is?

Dan Staples
Director, Solid Edge Product Development

Re: What is included in solid edge classic

Honored Contributor
Honored Contributor

I was not aware libraries could be purchased separate. Can any post a link here to a list of available part libraries? When looking at the original purchase, I decided adding about $500 year maintenance was not worth the 40 cross sections I had to create of steel that I actually use. For piping I have found Mcmaster Carr to be a great source as all common pipe fitting are there for free download.

 

I ended up with the fundamental version. As I'm still a noob on the scale of thing, I didn't see any reason to even move up to the classic.

 

As a result, I have no Idea what insight does or what libraries comes with classic.