Cancel
Showing results for 
Search instead for 
Did you mean: 

What is the cost savings of using Solid Edge Wire Harness

Valued Contributor
Valued Contributor

Does anyone have supporting information about time and cost savings (comparison) for using the Wire Harness capabilities of Solid Edge vs 2d wire harness work?

Nathan M. Gardner

https://www.etsy.com/people/NathanMGardner

Be sure to check out my work!!
Made in Maine Wood Carvings

5 REPLIES

Re: What is the cost savings of using Solid Edge Wire Harness

Gears Phenom Gears Phenom
Gears Phenom

Your VAR or Siemens Rep should be able to provide such data.

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: What is the cost savings of using Solid Edge Wire Harness

Phenom
Phenom

Matt is correct. But fist things first. Are you using an ECAD system already or are you just looking to run individual tube paths as wires?

Re: What is the cost savings of using Solid Edge Wire Harness

Valued Contributor
Valued Contributor

Right now, we are using nothing. our skematics and harness diagrams are created in 2d with alot of manual layout out the harnesses on a finished unit.

Nathan M. Gardner

https://www.etsy.com/people/NathanMGardner

Be sure to check out my work!!
Made in Maine Wood Carvings

Highlighted

Re: What is the cost savings of using Solid Edge Wire Harness

Gears Phenom Gears Phenom
Gears Phenom

@ngardner   aside from cost...  the wireharness does provide functionality and associtivity....  auto BOMS,  Connector tables, etc...    so, where accuracy and revisons come in,,,  time = Money right...

 

I would ask your VAR for a very specfic demo and a trial liscense and give it a whirl for 30 days

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: What is the cost savings of using Solid Edge Wire Harness

Siemens Genius Siemens Genius
Siemens Genius

Nathan,

I had a quick look through our published case studies and did not see any specific savings metrics for using the wire harness design capabilities - I think this is mostly because a lot of manufacturers forget to do a before and after performance analysis when they invest in a software solution - even when this would help them a lot the next time they go to the boss to ask for an investment!

You can do a search on the Solid Edge case studies web page for case studies that inlude references to "electrical" or "routing" for example: 

https://www.plm.automation.siemens.com/en_us/about_us/success/plm-case-studies/solid-edge.shtml?q=ro...

- then you can see the type of benfits these users are claiming - but they tend to be statements like "faster" and "we only needed to create one prototype"

Hope this helps...

Dave

{David Chadwick}, {Solid Edge Portfolio Development}, {Siemens PLM Software}