Cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between SharePoint inside solid edge(free) with the purchase SP

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

If we purchase Solid Edge, and inside the data management for Solid Edge, there will be SharePoints.

 

Is there any difference if purchase SP separately compare get from Solid Edge installer?

14 REPLIES 14

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

you can have an hour discussion on it but I will make it short

 

Solid Edge SP is more or less the Teamcenter concept based on the SharePoint Infrastructure. You have the Item/ItemRevsion thing. To view the content a license is alwasy needed.

 

Solid Edge Insight is the 100% SharePoint concept. You have a list with the Contentyp "Solid Edge Document". The list can have different views depending on who you are or what your are lookking for. To view the content no extra license is needed.

If you have othe SharePoint Solutions (Apps) eg. CRM this will fit 100%

 

Stefan

 

 

smitsch@unitec.de
www.all4edge.de

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Siemens Genius Siemens Genius
Siemens Genius

We have a matrix that highlights some of the key differences between Solid Edge Insight and Solid Edge SP - hopefully this will help answer your question

 

Also - when we launch Solid Edge ST9 on 16th May we will be talking about some new built-in data management capabilities in Solid Edge so look out for that

 

Dave

 

insight solid edge sp.jpg

{David Chadwick}, {Solid Edge Portfolio Development}, {Siemens PLM Software}

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@DavidChadwick, What is the cost difference? Or perhaps I should ask, what is the cost adder for SESP over Insight?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Siemens Genius Siemens Genius
Siemens Genius

Solid Edge SP is around $1k per seat if you are adding it to a Solid Edge Classic seat, a bit more if adding it to Solid Edge Foundation. As you probably know, Solid Edge Insight is included with Solid Edge Classic.

{David Chadwick}, {Solid Edge Portfolio Development}, {Siemens PLM Software}

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Thanks for the reply.

I will study more deeper on this and will back to you guys later.

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
@DavidChadwick as I review Insight itself got two types in ST8. One is Insight and another one is Insight Connect.
What is the difference between this two? Both are free when purchase Classic. Is it the functionality is different?

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Insight Connect is always a part of a Solid Edge Classic installation. So if you have Solid Edge installed Insight Connect is also installed

It can be purchased as a separated product if there are individuals with the need to do some administration work in Insight but they do not have Solid Edge Classic eg. Leader of the engineering team etc.

 

Here is a little overview about the functions:

- Start the Lifecycle of a part

- Do a revision of documents

- do a review of a document (measure, add remarks, etc)

 

Stefan

 

smitsch@unitec.de
www.all4edge.de

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Siemens Genius Siemens Genius
Siemens Genius

Just to add to Stefan's contribution - Insight Connect performs a lot of the operations of Solid Edge Insight but in a client that can run independently of the Solid Edge CAD software

 

Quoting from the Insight brochure:

"Solid Edge extends the power of Insight to users of design data through Insight Connect, the powerful Solid Edge design management client. Included with every copy of Solid Edge and also available as a standalone client, Insight Connect provides powerful design management functionality such as revision management, document lifecycle management and “where-used” searches. Insight Connect also provides powerful design review capabilities for consumers of design data, making it possible for extended team members to view multiple 2D and 3D file types – from Solid Edge and other sources – and interrogate the design using dynamic sectioning and measurement tools. Comprehensive markup capabilities can then be used to add comments."

 

We are working on including some of these capabilites in the core Solid Edge CAD software - look out for more info on this in the Solid Edge ST9 launch on May 16th

 

Dave

{David Chadwick}, {Solid Edge Portfolio Development}, {Siemens PLM Software}

Re: What is the difference between SharePoint inside solid edge(free) with the purchase SP

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
hai @DavidChadwick

ST9 just release new Built In Data Management, is it something that can replace Insight?or Insight is much more powerful compare to Built In Data Management?