Cancel
Showing results for 
Search instead for 
Did you mean: 

What's your favorite new thing in ST9?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Now that ST9 is released and people can download and start using it, please feel free to post your favorite new thing you have found in ST9.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com
44 REPLIES

Re: What's your favorite new thing in ST9?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's hard for me to pick just one thing, so I'll start off with a few things:

  • UI changes - The new App menu, the window tabs,
  • Multi-body changes - features now cut through multiple bodies
  • Display ordered body in Synch mode
  • Blocks in sketches
  • Design intent relationship - Maintain Offset Faces
  • Assembly Relationship Manager
  • Isolate and Toggle Display in Assembly
  • Drawing views orientation edit after placement
  • Section Views full options edit after placement
  • Fast Search
  • Revision Manager finally redone - Design Manager!!!

Told you it was hard for me to pick to pick just one.  I've got more, trust me...

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: What's your favorite new thing in ST9?

Gears Phenom Gears Phenom
Gears Phenom

Sorry my friend I have no favorite new thing. I have to say, that Solid Edge ST9 is the best new version in the past years.

 

Fresh, cool, "tasty" like a glass of orange juice! Smiley Wink

Great job! Cheers!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: What's your favorite new thing in ST9?

Legend
Legend

ST9 had no really big things, it's more of an fine-tuning version with an lot of small good changes.

 

What I'm exiting about is:

  • Expansion of the occurrence properties.
  • Multi-core in draft (Pitty not for section but the beginning is there).
Sander
The Netherlands

Re: What's your favorite new thing in ST9?

Phenom
Phenom

Here's something simple but was a serious pain in the rump.

 

!!Part Painter resets Parasolid body color!!

 

Having to deal with NX, SW and other Parasolid based CAD tools this is a major win. Simple solution to an old problem.

 

Re: What's your favorite new thing in ST9?

Phenom
Phenom

Support for high-resolution monitors

Solid Edge ST9 has improved support for bitmaps, controls, and other graphic elements displayed

on high-resolution monitors (3K, 4K, and higher). Although high-resolution monitor support is

available for both Microsoft Windows 7 and Windows 10, Windows10 offers superior dots-per-inch

(DPI) scaling capabilities.

 

This is a good move forward in support of touch devices with higher resolution screens and the newer xK monitors but I truly wish that there was a simple tool like a slider that you could use to change the resolution. This slider would then set the appropriate settings in Solid Edge and Windows Settings. It's a good first step I'd just like to see it better "packaged".

Re: What's your favorite new thing in ST9?

Honored Contributor
Honored Contributor

I will be installing tomorrow. I hope it speeds up gage table related problems that have been around for ST7 and ST8.

 

Re: What's your favorite new thing in ST9?

Gears Phenom Gears Phenom
Gears Phenom

I hope the material table is now sortable.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: What's your favorite new thing in ST9?

Legend
Legend

Export as excel file and sort with excel functions... its not the best solution but it works when you are like us and have nearly 200 materials to juggle when a new one gets added.

Re: What's your favorite new thing in ST9?

Siemens Phenom Siemens Phenom
Siemens Phenom

From page 3-2 of the Solid Edge ST9 What's New document:

 

"Sorting the material tree by ascending or descending material names..."

 

2016-07-19 07_58_05-whatsnew.pdf - Adobe Acrobat Reader DC.png