Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

What version of Creo file/ProE can be open in Solid Edge ST9?

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi Edgers,

 

I have a potential client that using Creo before an ask what version of Creo that Solid Edge can open.

 

BTW, since Creo and ProE is the same product with same extension file, is there any issue for solid edge to open this file?

3 REPLIES

Re: What version of Creo file/ProE can be open in Solid Edge ST9?

Valued Contributor
Valued Contributor

I can open 3.0 files in ST9.  No model tree of course.  The front plane in Creo will be the bottom plane in ST9.  Creo just released 4.0 recently but I doubt ST9 will open that version.

 

Matt

Re: What version of Creo file/ProE can be open in Solid Edge ST9?

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
Hey thanks for the sharing.

Is there any documentation I can get from Siemens regarding to which version Creo file can be open in Solid Edge.
Then it easier for me to show clients.

Re: What version of Creo file/ProE can be open in Solid Edge ST9?

Siemens Phenom Siemens Phenom
Siemens Phenom

My first source would be the SE Help:

" Siemens Documentation: Opening Pro/Engineer Documents in Solid Edge

The translator for the Open command and the Proe Migration Wizard supports Pro/Engineer files created in ProE version 17 - Creo Parametric 3.0."

 

Siemens EMEA GTAC Support