When I try to do an extrude of a simple circle the program says it has to quit.

Creator
Creator

When I try to extrude a simple circle the program says it has to quit. Is this a video driver problem?

 

thanks

8 REPLIES

LC,   This could be a few different thing, one of which c...

Esteemed Contributor
Esteemed Contributor

LC,

 

Could be a few different things going on there, one of which could indeed be the video performance &/or driver.

 

Something to try, would be reducing the Solid Edge display settings...from within an new part file, go to Application Button > Solid Edge Options > View tab, uncheck the "Automatic selection" and from the drop down menu, choose "Backing store".

 

SE_Options_View_ApplicationDisplay.png

 

HTH.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: LC,   This could be a few different thing, one of which c...

Creator
Creator
I applied the change but got the same result.

Re: LC,   This could be a few different thing, one of which c...

Esteemed Contributor
Esteemed Contributor
Could you give details of your system specs? [Make & model, CPU/Hard drive type/RAM/Video card type]....this will hopefully help nail down the cause & possible sollution.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: LC,   This could be a few different thing, one of which c...

Creator
Creator
sending email

Re: LC,   This could be a few different thing, one of which c...

Creator
Creator
Can't get email to send. So here is info.

Acer- A0722
CPU- AMD c-60 APU (core 2 duo)
Video- Radeon HD 6290 1.0 Gb
Ram- 4G
HD- 320G
Windows 7 Pro 64 bit

Another window:
Total available graphics memory 1909 MB
Dedicated graphics memory 256 MB
Dedicated system memory 0 MB
Shared system memory 1653 MB

Re: When I try to do an extrude of a simple circle the program says it has to quit.

Esteemed Contributor
Esteemed Contributor
Switch it to software rendered.

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: LC,   This could be a few different thing, one of which c...

Creator
Creator
Same result. Just blows up. I will check back often. If there are any more ideas I will give them a try. thanks for trying.

Re: LC,   This could be a few different thing, one of which c...

Esteemed Contributor
Esteemed Contributor
Hi there,

I see that the HD 6290 graphics actually lists as having no dedicated memory and relies on shared memory for any performance. [ http://www.notebookcheck.net/AMD-Radeon-HD-6290.51810.0.html ]
So when running a graphics intensive application like Solid Edge on a Netbook such as the AO722, this is probably asking a bit much of it.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000