Cancel
Showing results for 
Search instead for 
Did you mean: 

When placing origin of text box or string, is there a way to have it snap to the grid or an element

Creator
Creator

I’m using Solid Edge 2D Drafting ST5:

1) When placing origin of text box or string, is there a way to have it snap to the grid or an element keypoint?

2) I’ve set the option to automatically save document every 30 minutes, but it always reminds me: “You have not saved your documents recently. Save all documents now?” Is there a way to make this fully automatic, so it does not have to ask, and simply saves documents?

Thanks

1 REPLY

There are 2 options for AutoSave: Save the file Create a...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are 2 options for AutoSave:

  1. Save the file
  2. Create a backup copy

If you choose the Save the file option, it prompts you because sometimes you make changes that you don't want to save.

 

If you choose the Create a backup copy option, it is completely automatic and it's purpose is in case a crash happens, you do not lose all your work.  SE is able to pick up the backup copies and restore them when it restarts.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com