Cancel
Showing results for 
Search instead for 
Did you mean: 

When you create a .dxf in Solid Edge and open it in Autocad all the lines are white?

Creator
Creator

When I create a .dxf in Solid Edge and open it in Autocad all the lines are white. Is there a way to carry over the line colors in Solid Edge to Autocad?

1 REPLY

In the Options Wizard (Option button when you set file of...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In the Options Wizard (Option button when you set file of type to DWG) there is a page for width to color mapping.  The option to do that defaults to on and it is all set to color "7".  Just turn off the option (check box).



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com