Cancel
Showing results for 
Search instead for 
Did you mean: 

Where are callouts saved and how do I copy them?

Valued Contributor
Valued Contributor

My colleague has loads of saved call outs - making drafting easier when adding things like notes to drawing.

 

How can he send them to me?

Is it possible to save them to the template 

Regards,

MagRiz
(ST9 User Est 01.18)
5 REPLIES

Re: Where are callouts saved and how do I copy them?

Gears Phenom Gears Phenom
Gears Phenom

[Solid Edge Install Location]\Template\Reports\draftcallout.txt


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Where are callouts saved and how do I copy them?

Gears Phenom Gears Phenom
Gears Phenom

Consider mapping to a shared file via File Locations from SE Settings ->  Options -> File Location


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Where are callouts saved and how do I copy them?

Valued Contributor
Valued Contributor

@Johnson_BigMatt

 

Thanks, yes that would be better as ideally i would like everyone in the company to use these callouts.

 

 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Where are callouts saved and how do I copy them?

Valued Contributor
Valued Contributor

When i'm saving call outs the font size doesnt save. I set it to 8 and save it but when i use the callout it reverts back to 3

 

edit: also callouts that were saved without leaders are showing leaders, the only thing that seems to have saved is the text only. 

@Johnson_BigMatt

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Where are callouts saved and how do I copy them?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

text style, text size etc. is a matter of the used Format Style!

And those are saved within Your document (template)

 

 

 

regards
Wolfgang