Cancel
Showing results for 
Search instead for 
Did you mean: 

Where used and Open Drawing broken after WIN 1803

Phenom
Phenom

Any suggestions? Design Manager seems to have given up the ghost, thanks to the WIN 1803 update. FWIW this update switched indexing off, after which I switched it back on. 

 

Thanks/Harri

 

8 REPLIES 8

Re: Where used and Open Drawing broken after WIN 1803

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Was the indexing being switched off the only issue?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200
Highlighted

Re: Where used and Open Drawing broken after WIN 1803

Phenom
Phenom
The only issue Windows reported. My issue is Design Manager not working ;(

Re: Where used and Open Drawing broken after WIN 1803

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You don't specify in what way DMan is not working.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Where used and Open Drawing broken after WIN 1803

Phenom
Phenom
Sorry, it was only in the title.. open drawing finds nothing, as does where used. Might be other troubles too, haven’t had time to investigate.

Re: Where used and Open Drawing broken after WIN 1803

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't use BiDM but indexing sounds like the key ingredient. Has it had time to rebuild the index?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Where used and Open Drawing broken after WIN 1803

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are times where Windows updates remove the Solid Edge properties from the Indexer.  You also need to make sure your folder you are using are set to be indexed.

 

To add the SE props back, 

Run CMD in administrator and after run :
regsvr32 "C:\Program Files\Solid Edge ST10\Program\sepropertyhandler.dll”



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Where used and Open Drawing broken after WIN 1803

Phenom
Phenom

@KennyG

 

YES, YES, YES!!! Success. Thank you, would never have figured that out.

Re: Where used and Open Drawing broken after WIN 1803

Phenom
Phenom

@bshand,

 

thanks for pointing this out, took almost an hour to complete..