Why are some templates greyed out when I select from New under the application icon?

Valued Contributor
Valued Contributor

What's strange is that if I move them around in the listing, they will become active.  Another annoyance is that I make the change and they do not "stick".  Even though I made sure that the check box did NOT have a check in it.

 

new templates.JPGtemplate.JPG

3 REPLIES

Re: Why are some templates greyed out when I select from New under the application icon?

just a guess....   UAC setting.   you may not have write permissions to the template folder.?

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6

Re: Why are some templates greyed out when I select from New under the application icon?

Siemens Phenom Siemens Phenom
Siemens Phenom

There is a known issue in ST9 that when the number of templates exceed sixteen, then the seventeenth and higher will not behave correctly in the New screen.


Should be fixed in ST9 MP5. 

Re: Why are some templates greyed out when I select from New under the application icon?

Valued Contributor
Valued Contributor

I created some additional folders to put templates in and now I'm at 16 and it's working.