Cancel
Showing results for 
Search instead for 
Did you mean: 

Why do I get 2 drawings when clicking on "Drawing of Active Model"?

Hi you Smiley Happy

 

I hope one of you might be able to help me with an odd problem.

Why do I get 2 drawings when I just one to make one?

 

I use the 

 

7 REPLIES

Re: Why do I get 2 drawings when clicking on "Drawing of Active Model"?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
It is most likely because that model was inserted as a drawing view in both drawings. It is essentially performing a where used on the active model and filtering the results to just DFT files.


Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Why do I get 2 drawings when clicking on "Drawing of Active Model"?

It's a new part and its the same for all parts I make, even sheet metal.

Highlighted

Betreff: Why do I get 2 drawings when clicking on "Drawing of Active Model"?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Maskinbyggerne

 

 

 

OK, it has taken just a couple of minutes to see it, but there are not two drafts of Your parts, there are only two views of the same draft file - so called "Multi Window"

You can see the same file name for both draft tabs.

 

And now the question comes up: "Why?"

 

Answer - I just have tested it here - You have saved Your draft template with two windows opend, and therefore it comes back with two windows open.

 

Just save Your tempalte with only one window and everything will be as usual!

 

 

regards
Wolfgang

Betreff: Why do I get 2 drawings when clicking on "Drawing of Active Model"?

Wow.... that was brilliant - that was the exact reason for my problems !

 

I hope Siemens pay you for all the help you provide on this forum, it's insane.

Thanks again - have a great evening Smiley Happy

Betreff: Why do I get 2 drawings when clicking on "Drawing of Active Model"?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Maskinbyggerne

 

 

welcome!

And no, but the acknowledgement of people like You is the payback and motivation for all those efforts.

 

I cann't deny, I'm an EdgelingSmiley Wink

 

regards
Wolfgang

Betreff: Why do I get 2 drawings when clicking on "Drawing of Active Model"?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Don't forget to mark his post as the solution.  It'll help other Edgelings in the future.


____________________________________
--Scott Wertel, P.E.

Betreff: Why do I get 2 drawings when clicking on "Drawing of Active Model"?

Already did that yesterday, so think all is ok Smiley Happy