Cancel
Showing results for 
Search instead for 
Did you mean: 

Why do I have check every view when updating a configuration

Gears Phenom Gears Phenom
Gears Phenom

I use  a lot of view configurations when creating assembly drawings.  The problem is when I change a configuration in the model, I have to go to every view that uses it, open the properties dialogue, go to display, hit the check button then update the view - over and over and over.  If I have "match" already checked, why is it necessary to check it again?  SE should automatically do this and put the gray box around the view ready for me to hit the update button.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1
5 REPLIES

Re: Why do I have check every view when updating a configuration

Phenom
Phenom

There is a switch for this:

 

SE Button

- SE Options

-- General Tab

--- 3/4 of the way down, put a check next to "Assembly configuration changes make drawing - --- views out of date in the draft file"

 

That should take care of the problem.

 

HTH,

 

Bob Henry

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Why do I have check every view when updating a configuration

Gears Phenom Gears Phenom
Gears Phenom

Thanks Bob,

 

That should save a lot of time.  I wonder why that setting is not the default?

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Why do I have check every view when updating a configuration

Phenom
Phenom

No idea why it is not default. This switch was not always there. I can't recall what version it came in, but it was a pretty long time ago, maybe the early teens?

 

Bob

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Why do I have check every view when updating a configuration

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
I believe it is is a performance issue. We have this option turned on in the template we use for parts explosions (config based) and turned off in our main template (normally not config based.)

Jason

Re: Why do I have check every view when updating a configuration

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think the SE guys are also careful to make sure that when they add new stuff that changes a behavior such as this, that change is not introduced by default as it may negatively effect a workflow that some people may have.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com