Cancel
Showing results for 
Search instead for 
Did you mean: 

Why do elements mirrored across a centerline (annotation) not have automatic symmetry?

Experimenter
Experimenter

When I mirror elements across a regular line (draw group) they have a symmetric relation automatically. Why is it when I do this with a centerline (annotation group) there is no automatic symmetry applied?  You would think it would.  Thanks.

1 REPLY 1

Re: Why do elements mirrored across a centerline (annotation) not have automatic symmetry?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @CR1,

 

Because the centerline is, as you point out, an "annotation", and as such only gets momentary positioning reference, whereas if you use a sketch line, that physical geometry is then able to persistantly drive the mirror axis, giving the user automatic symmetry by the system.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000