Cancel
Showing results for 
Search instead for 
Did you mean: 

Why is the mid surface command in multi body and not the surface tab

Gears Phenom Gears Phenom
Gears Phenom

I'm working on an analysis of a sheet metal bracket and need to create a mid surface.  The command is buried in the multi body pull down.  This command should be with all of the other surfacing tools.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1
1 REPLY

Re: Why is the mid surface command in multi body and not the surface tab

Honored Contributor
Honored Contributor

First guess, so you can use the mid surface to split a body appart into multiple bodies.