Cancel
Showing results for 
Search instead for 
Did you mean: 

Why won't the hole callout command display any information about the hole?

Pioneer
Pioneer

I am just trying to callout simple holes and counterbores.  When I select the specific hole that I want to callout nothing but %HC appears, or anything symbol that I enter manually.  In the callout properties the Hole Callout tab is completely blank.  I am using a template an engineer has already set up, and I realize in a new solid edge template there is actual formulas filled out in the hole callout tab.  Do I have a broken link to a template or something like that?  Sorry if someone has asked this before.  Thanks in advance Smiley Happy

3 REPLIES

Be advised...  you feature must be a true HOLE...  not a...

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Be advised...  you feature must be a true HOLE...  not a cut out for %HC to work.

 

if this is so... then yes, it appears that your template is not complete.  We now use %HC as the generic way of calling out a hole and this allows us to be more specfic on the feature callout tab... 

 

check your feature call out tab to assure it is populated.

 

Quick check would also be to place your part in a standard template and test.

http://screencast.com/t/5tQMiVhLBGS1

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: Be advised...  you feature must be a true HOLE...  not a...

Pioneer
Pioneer
Thank you for the reply. The call out tab is definitely not populated. When I try to populate that list similar to what a blank Solid Edge template has, it doesn't save the input. I checked the Holes.txt file which is what I assume SE references for callouts, and it is set for that file in File Locations under SE options. There is also a Holes_old which I assume is from a previous version.

Re: Be advised...  you feature must be a true HOLE...  not a...

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
be advised that with Windows UAC you may not have write access to the C:\Programs folder...

Advised to turn off UAC or Install Solid Edge somewhere other than C;\Programs folder...
Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/