Cancel
Showing results for 
Search instead for 
Did you mean: 

Will this laptop be able to run ST10? i7 with K3000M

Valued Contributor
Valued Contributor

Hi,

 

I'm thinking about buying this used laptop:

Will it be able to run ST10?

 

HP EliteBook 8770w

- i7, 2,6Ghz

- 8 GB RAM (will upgrade to 16)

- 180GB SSD HD
- Rigtig god/kraftig & stabilt business bærbar fra 2013
- 17!, 1920x1080
- Quadro K3000M

 

Udklip.PNG

9 REPLIES 9

Re: Will this laptop be able to run ST10? i7 with K3000M

Phenom
Phenom

hi @Kenneth that looks like a decent machine. Note the processor can ramp up to 3.6Ghz when it's underload which is good. 

 

Just note that it takes very little power to run Solid Edge itself, what you need power for is dependant on the size and complexity of your models. This means that it's impossible to say how it will be in real life on your data without you trying it! But as I said, that looks like a decent machine either way.

 

Betreff: Will this laptop be able to run ST10? i7 with K3000M

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kenneth

 

 

 

specifications sounds better than many desktop computers I have seen in the last couple of years.

Maybe accept of the memory.
Here will an upgrade to 16GB or 32 GB be definitefely an enhancement.

On the other hand, depending on Your models, who knows wether the 8GB will be used completely.

 

 

regards
Wolfgang

Re: Will this laptop be able to run ST10? i7 with K3000M

Valued Contributor
Valued Contributor

Thanks for the replies.

I have bought the computer and waiting to receive it Smiley Happy

Re: Will this laptop be able to run ST10? i7 with K3000M

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kenneth

 

 

 

let us know how it works!

 

If possible, You can let run the SE Performance test and You can share the results here.

 

regards
Wolfgang

Re: Will this laptop be able to run ST10? i7 with K3000M

Valued Contributor
Valued Contributor

Awesome, will do that Smiley Happy

 

Where do I find that tool?

Re: Will this laptop be able to run ST10? i7 with K3000M

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kenneth

 

 

 

just go to the download area of Solid Edge, where YOu also find the Maintenance Packs, and look for "Support Tools"

 

Here You will find the "PerformanceTool.exe".

Download, unpack and give it a try.

The results will be stored and can be shown.

Would be great to see them here, it always is good to knwo which ahrdware specs should be used for further equipement

 

20171027_0835.PNG

regards
Wolfgang

Re: Will this laptop be able to run ST10? i7 with K3000M

Valued Contributor
Valued Contributor

Perfect, thanks again !

Re: Will this laptop be able to run ST10? i7 with K3000M

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It has been only 3 or 4 years since then but I was using a Pentium 4 machine with no special graphics card and 4 or 8 GB ram. Accessing files over the internet via Teamcenter because I was working from home at the time. Big models too. It wasn't that bad. I would think that laptop will be fine.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Will this laptop be able to run ST10? i7 with K3000M

Valued Contributor
Valued Contributor

I'm running ST9 with;

 

Hewlett-Packard EliteBook 8770w

i7-3610QM CPU @2.30GHz

16Go RAM

nVidia Quadro K3000M

 

Work perfectly for SE even with large assembly but the K3000M seems to overheat with Keyshot.

 

I'll run ST10 on a;

HP ZBook 17 G3

Xeon CPU E3-1575M v5 @ 3.00Ghz

16Go RAM

nVidia Quadro M3000M

 

we'll see. ;-)

Good Marketing makes the company look smart.
Great Marketing makes the customer feel smart.