Cancel
Showing results for 
Search instead for 
Did you mean: 

Win 10 update causing SE9 crash

Legend
Legend

We had a problem today with SE9 crashing in assembly mode. We called the VAR and they had us delete the regestry entries but the problem came back. We noticed there was a new update, we rolled it back and now it seems to be working. It's a little tricky to roll back the update beecause you have to shut off auto-update and that is very well hidden now.

 

Has anyone else had the same problem?

 

Larry

Using SE since V12, 2002
ST10 certified
3 REPLIES

Re: Win 10 update causing SE9 crash

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @lking,

 

Not seeing that issue here, Larry.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP3] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Win 10 update causing SE9 crash

Valued Contributor
Valued Contributor

The problem arose in connection with the Win10 Update.
It was not automatically updated when you release it to show the Part Libruly window.
This occurred after a Windows update.
People also do not use any window to hide the problem? ...
Clearly there is a problem regarding the Update.

Re: Win 10 update causing SE9 crash

Legend
Legend

We ended up "re-setting" Win 10. Winspeak for disk wipe and reinstall, but now they have an app that does it for you. It changed the CID for the SE license so we had to get a new license file.

Using SE since V12, 2002
ST10 certified