Cancel
Showing results for 
Search instead for 
Did you mean: 

Windows 10 update. Plugging issue (ST8)

Experimenter
Experimenter

After the last update, the program is continuously frozen. It's not a problem at first. As time goes by, the frost is increasing.

7 REPLIES

Betreff: Windows 10 update. Plugging issue (ST8)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @cagdas

 

 

 

can You further specify what exactly is going on, and which Update are You referring to?

General or Fall Creators Upate?

 

If Fall Creators Upate, You should follow the several other posts here, since there are more than one issues coming in with Win 10 Fall Creators Update, but as I have seen here, we might expact an Service Pack from Microsoft next week, hopefully

 

 

regards
Wolfgang

Betreff: Windows 10 update. Plugging issue (ST8)

Experimenter
Experimenter
System features:
https://i.hizliresim.com/m2Gam2.png

When I move the fragment to the 2D environment, the commands are opening late. The icons come one by one.

Betreff: Windows 10 update. Plugging issue (ST8)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You have the Fall Creator's update and your symptoms match.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Windows 10 update. Plugging issue (ST8)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@cagdas  Microsoft released the Fall Creators Update (version 1709) with a bug that causes 2D graphics memory to fragment badly which causes a severe performance degradation.  Microsoft has stated that there should be a fix released on or about January 23rd. In addition, Solid Edge is going to be releasing Maintenance Patches soon to workaround the Windows 10 bug.  In the meantime you can either roll back the Windows update or reboot when the perfprmance gets too bad.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Windows 10 update. Plugging issue (ST8)

Genius
Genius

Has anyone heard anything regarding problem? seeing how the suggested time frame has come and gone.

Betreff: Windows 10 update. Plugging issue (ST8)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It was reported that the Microsoft patch was rescheduled for 1/30, but no word on how to get it...



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Windows 10 update. Plugging issue (ST8)

Genius
Genius
thx



Thank You,



Bob Haskin KE7-TSA

Pacific Design Service



27906 V Street

Ocean Park, WA 98640



H: 360-665-2354

C: 360-244-1741

bh41@willapabay.org

Skype: bob.haskin1