Cancel
Showing results for 
Search instead for 
Did you mean: 

Wiring diagram symbols

Experimenter
Experimenter
I cant find these symbols any where numbers 90 and 93 94 and 95 99 and 100
3 REPLIES 3

Betreff: Wiring diagram symbols

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Jd3

 

 

have You looked into the sample block files in the Solid Edge folder ?

 

C:\Program Files\Siemens\Solid Edge 2019\Sample Blocks\Electrical

 

20181020_2038.png

 

There are several block drafts including alot of symbols.

And if they are not included, then You can use any vlock library from Autocad (DWG/DXF) and if they are not available too there, then You can create Your needed blocks Yourself very easy.

 

 

regards
Wolfgang

Betreff: Wiring diagram symbols

Experimenter
Experimenter
Where do I find the files I haven't used this site much

Betreff: Wiring diagram symbols

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Jd3

 

 

I have copied the path to them:

 

C:\Program Files\Siemens\Solid Edge 2019\Sample Blocks\Electrical

 

 

20181020_2112.png

regards
Wolfgang