Cancel
Showing results for 
Search instead for 
Did you mean: 

Wirng Harness

Creator
Creator

Is there a way to create a wiring harness (by using the wiring harness feature) in a subassembly, and still be using wiring clamps that are in the TLA?

4 REPLIES

Re: Wirng Harness

Creator
Creator

I mistyped I meant to say us the clamps and a routing point.

Re: Wirng Harness

Siemens Phenom Siemens Phenom
Siemens Phenom

While IPA at the subassy level, if you hold the Shift key down, you should be able to select keypoints on components at the TLA.  Is this what you are looking for?

 

 

Kevin Grayson
Solid Edge Technical Consultant
kevin.grayson@siemens.com

Re: Wirng Harness

Genius
Genius

I do this that in assembly I make wire harness, and in subassembly (where it should be wire harness that I make in higher level of assembly) I put an empty part witch number of a wire (such a small misrepresentation Smiley Happy )

 

I once tried to make use of the adjustable assembly but completely it has not happened.
 
It should be possible to edit a subassembly with wire harnes, depending on the assembly where it is located.
SE ST9 + TC 10.1.7

Re: Wirng Harness

Creator
Creator

Thanks for the quick response.