Cancel
Showing results for 
Search instead for 
Did you mean: 

Wood Plastic Composite In Material Table

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I notice on the material table there is ABS High, Medium Plastic, Acrylic Plastic. Are any of these the same as Wood Plastic Composite?

 

Thanks

Greg 

3 REPLIES

I believe you answered your own question when you asked i...

Phenom
Phenom

I believe you answered your own question when you asked if they were 'the same as something different'.

-Dylan Gondyke

Greg, No, they are different.....I'm not 100% sure, but...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg,

No, they are different.....I'm not 100% sure, but I think Student Edition does not allow you to create your own material [to those pre-loaded] definitions, as you would need to in this case.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Greg, wood/plastic composite is typically an extruded the...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg, wood/plastic composite is typically an extruded thermoplastic (PolyVinylChloride, PolyPropelene, PolyEthylene) with wood flour or fiber mixed in as a filler.  Since it is a composite and the formulas vary widely in the mixture, the mechanical properties are very specific to a particular brand/product.  You would surely need to create the material your self.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com