Cancel
Showing results for 
Search instead for 
Did you mean: 

Wrapping Around A Cylinder

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

With This Image, I Am Attempting To Wrap Around This Rectangle To A Cylinder... I Would Love To Send A Short Video, But, Then Again I Do Not Know Where To Start.

 

Thank You

GregoryLee Crouse

http://screencast.com/t/sWqu2gu5 

5 REPLIES 5

Re: Wrapping Around A Cylinder

Valued Contributor
Valued Contributor


Hello GregoryLee,

 

I myself am a new learner. So I don´t know how to wrap a solid around another solid. Furthermore, as far as I remember, you cannot have two tangent solids, (I mean in the same part, as it will give you a zero thickness error). Anyway, I think you can do it in another way, I have attached a short video so that you can see it.

 

Good luck!

Re: Wrapping Around A Cylinder

Gears Phenom Gears Phenom
Gears Phenom

i do not that you can actually "wrap" this in SE but you will need to model it in its formed position.   you could alternatively use sync and rotate the face around they cylinder.

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Wrapping Around A Cylinder

Gears Phenom Gears Phenom
Gears Phenom

heres a short video of using Sync...  to "wrap" 

 

be aware that the the cylinder and the recangular extrusion can not have a boolean so in my model there is .0001 gap.

 

http://screencast.com/t/VcKFO13q

 

open in internet Explorer to view...


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Wrapping Around A Cylinder

Phenom
Phenom
Very interesting video!

Then if you try to extrude the same sketch, you'll not be able to do it... Zero thickness...

On the other hand revolving is possible Smiley Wink

Yasser

Re: Wrapping Around A Cylinder

Valued Contributor
Valued Contributor

Do you want the bent/wrapped rectangle part and the cylinder to be one solid or do you need a gap between them?